Technical FAQs

Ask a Question

What is the meaning of the ``MT`` on the end of an FI36100MT I-Line circuit breaker?

The ``MT`` suffix on this breaker indicates that the I-Line plug-on assembly is mounted at the ``OFF`` end of the breaker, and the lugs are mounted at the ``ON`` end.

CTA-ID : 2019300
Was this helpful?
What can we do to improve the information ?