Technical FAQs

Ask a Question

On a Merlin Gerin Master Pact MP08H1 type 800A breaker, can the trip settings on the control unit be adjusted with the breaker energized?

Square D recommends that the breaker be de-energized before any settings are changed. Adjusting them with the breaker energized carries a small risk of breaker tripping, depending on loading and settings changed.

CTA-ID : 2019299
Was this helpful?
What can we do to improve the information ?