Technical FAQs

Ask a Question

Will a QOMB3 accept single pole breakers?

Yes, can use (3) single pole OR 1-single pole with (1)-2pole OR (1)- 3pole breaker(s).


CTA-ID : 2019294
Was this helpful?
What can we do to improve the information ?