Technical FAQs

Ask a Question

What are the differences between the C60N and NC100 lines ?

The C60N has a 5kAIC rating at 480Y/277v ( vs. 10kAIC ) , has more B & C curve options and is rated up to 63a max (vs. 80a) . The C60N has a few more accessories as well .

CTA-ID : 2019293
Was this helpful?
What can we do to improve the information ?