Technical FAQs

Ask a Question

What is th maximum available VA rating for the 9070KL (Type K with leads) control transformers?<br />

300 VA is the maximum available rating. (Submit a ``The Form`` if request involve a large quantity for an OEM.)


CTA-ID : 2020290
Was this helpful?
What can we do to improve the information ?