Technical FAQs

Ask a Question

What is the part number for the ventilation fan kit for ATV58HU29M2ZU, ATV58HU41M2ZU, ATV58HU18N4ZU, ATV58HU29N4ZU and ATV58HU41N4ZU ?

For clarification, these fan kits are accessory fan kits for use in applications with higher than normal ambient temperature. These fans are mounted at the top of the drives. They are used for Type H and Typ FVC products and are powered from the drive. These are not the same as the heatsink fans that are included on some drives and located at the bottom.

Reviewed 12/2011

CTA-ID : 2020288
Was this helpful?
What can we do to improve the information ?