Technical FAQs

Ask a Question

What are the repair parts for a QMB363T22WCRSLC, series E1?

This QMB device is a twin switch, meaning it contains two switches in one device. In this device, the fuse clips are 60A fuse clips. Parts are listed per switch. Only the parts below are considered field replaceable.
-Complete Arc Suppression Assembly - 3 part numbers required:
(1) Arc Suppressor Assembly (1 required) - 4052021450
(1) Arc Shield (top cover) (1 required) - 4052017302
(2) Push Nuts (2 required) - 2330241601
-Load Base Assembly (1 required, includes lugs) - 4052020650X01
-Load Base Mounting Screws (2 required per load base) - 4020506501
-Handle Knob Kit - 4028343750
-Lug Assembly (per lug) - 4025672850
-Lug Mounting (per lug) - 2342501700


CTA-ID : 2020286
Was this helpful?
What can we do to improve the information ?