Technical FAQs

Ask a Question

Is a 9422ATCF332 made of stainless steel?

The exposed metal parts of the handle mechanism 9422A2 are made of stainless steel or chrome plated non-ferrous die casting. The switch itself is not. The handle is the only part exposed to the environment outside the enclosure.

CTA-ID : 2019852
Was this helpful?
What can we do to improve the information ?