Technical FAQs

Ask a Question

How does one reset a PAF2036 ?

First crank the handle to the ``7 o`clock`` position from the tripped position at ``4:30 `` . Then crank the handle up to ``3 o`clock`` to ON . (The normal OFF position is at ``6 o`clock `` ).
The rating columns must be installed in order for the breaker to be reset.

CTA-ID : 2019850
Was this helpful?
What can we do to improve the information ?