Technical FAQs

Ask a Question

I have a spec calling for a 100% rated solid state full function 500 Amp breaker. Can I use an LEL36500LIG? Do I need to go to an M frame?

You will need to use the M frame or Powerpact P frame. The LE with a 600 A sensor is 80% rated regardless of the rating plug or Long-Time setting.


CTA-ID : 2018430
Was this helpful?
What can we do to improve the information ?