Technical FAQs

Ask a Question

Where can the EDS files for the ATS48 unit using LUFP9 Modbus to Devicent gateway be located?

Issue:
Where can the EDS files for the ATS48 unit using LUFP9 Modbus to Devicent gateway be located?

Product Line:
Altistart ATS48

Environment:
All

Cause:
Needs the EDS files for the LUFP9 gateway.

Resolution:
These files are included on the V2.0 PowerSuite CD part number VW3A8104.
or see the attached files.


CTA-ID : 2019010
Was this helpful?
What can we do to improve the information ?