Technical FAQs

Ask a Question

Can 460V 50hz line input power be used on 460V ATV58 drives?

460V 50hz power can be used on the ATV58HU18N4 to ATV58HD79N4 size drives but not on the ATV58HC10N4 and larger drives.
The High horse power units have transformer on the line side feeding power to the precharge circuit that only works with 60 Hz at 460 - 480 VAC.

CTA-ID : 2018864
Was this helpful?
What can we do to improve the information ?