Technical FAQs

Ask a Question

What should be done if the control voltage for the heater circuit must be 240VAC rather than the standard 120VAC.

Two heaters must be wired in series to drop 120VAC across each hearter. They must be placed in the switchgear so that the correct wattage is provided in each section

CTA-ID : 2018667
Was this helpful?
What can we do to improve the information ?