Technical FAQs

Ask a Question

Can a low voltage panelboard be mounted in a bus transition section of an HVL switchgear lineup?

No, the transition bus is also in the front of the section. It is best to mount the panelboard in a low voltage tub with door in an adjacent HVL section.


CTA-ID : 2018658
Was this helpful?
What can we do to improve the information ?