Technical FAQs

Ask a Question

What is the part number for a lug for the RL breaker?

See page Digest 173 page 6-43 and 6-44, or Accessories section of Class 612 Catalog for lug selections. There are lugs for I-Line and Unit mount construction.

CTA-ID : 2018373
Was this helpful?
What can we do to improve the information ?