Technical FAQs

Ask a Question

Can we build an NQ panel a split bus arrangement different from those on the product selector menu?

Issue:
Can we build an NQ panel a split bus arrangement different from those on the product selector menu?

Product Line:
Panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
Some additional bus arrangements may be possible, and should be verified by manufacturing before quotation. Although it cannot be selected on the ``product selector``, a special arrangement can be entered into the note pad and then a drawing showing the layout should be provided to the plant through the field office.


Revised 6/1/04


CTA-ID : 2018162
Was this helpful?
What can we do to improve the information ?