Technical FAQs

Ask a Question

Can he order just one replacement contactor for a 8810SCO12V02, two speed starter?<br />

Yes, he can. The top contactor is a 8502SCO2. If required the 2 pole (NO) Power Pole is a 9999SB9. The bottom starter is a 8536SCO3.

CTA-ID : 2035446
Was this helpful?
What can we do to improve the information ?