Technical FAQs

Ask a Question

Is it possible to have the Altivar 31 display the same parameter each time it is powered up?

To change the parameter displayed, scroll to the desired display parameter in the SUP menu and press the ENT key.  To retain your selection as the new default, press and hold the ENT key again for 2 seconds.  The value of this parameter will be displayed during operation, even after power to the drive controller has been cycled.  If the new choice is not confirmed by pressing the ENT key a second time, the drive controller will return to the previous parameter after power is cycled.

Reviewed 6/2011

CTA-ID : 2018992
Was this helpful?
What can we do to improve the information ?