Technical FAQs

Ask a Question

Are the Vario load break switches available in a Nema 3R enclosure?

No, they are available in NEMA 1, 12, and 4/4X (indoor only).


CTA-ID : 2018635
Was this helpful?
What can we do to improve the information ?