Technical FAQs

Ask a Question

Is the ambient temperature range of ATS01N2**LY different from LH4N2**LY7 as indicated in the June 2004 ATS01 catalog?

The temperature range for ATS01N2**LY is the same as the LH4N2**LY7 product: -10 to 55C.
The ATS01 catalog (as of June 2004) has a typographical error.
See attachment for a written confirmation from Product management.
NOTE: The link contains a document that is not for general distribution.
For details, contact Drive Products Support at 888-SQUARED or E-mail

Reviewed 10/2011

CTA-ID : 2018365
Was this helpful?
What can we do to improve the information ?