Technical FAQs

Ask a Question

Do QO and HOM load centers meet Federal Specification W-P-115-c Type 1 Class 2 ?

Issue:
Application

Product Line:
QO and HOM Load Centers

Cause:
Application, Standards

Resolution:
The QO and Homeline Load Centers did meet this Federal Specification, however the specification was rescinded in 2001.


CTA-ID : 2018579
Was this helpful?
What can we do to improve the information ?