Technical FAQs

Ask a Question

Can the Square D AFI circuit breaker provide ground fault protection where required by the NEC?

No. The AFI breaker will trip on a 30 to 50mA ground fault, but is not UL listed for either equipment or personnel protection.

CTA-ID : 2001878
Was this helpful?
What can we do to improve the information ?