Technical FAQs

Ask a Question

Why would the ATV58 drive will not accept PI setpoint through the N2 network. The setpoint reverts to `0` when a any new value is entered.

The Bulletin No. VVDED300028NA R5/02 contains an error on page 34 for table 4 network point address 6.
The PI setpoint over the N2 network is scaled by our option card to be 0 to 10, not 0 to 10,000 as our documentation suggests. 0 to 10 in increments of 0.1 correspond to the 0-10 VDC signal that would otherwise be used by PI control to represent 0-100% when controlling the drive through the I-O terminals.
Any value over 10 is invalid.


CTA-ID : 2017971
Was this helpful?
What can we do to improve the information ?