Technical FAQs

Ask a Question

What is the RJ45 pin out for the Altivar 31?

The RJ45 connector uses two wire RS-485 connection for Modbus communications.
Pin 4 is the DB (+). Pin 5 is DA (-). These terminals are for communication.
Pin 7 is 10 VDC and 8 is 0 VDC. These are used to power the remote keypad when connected to this drive or the RS232 to RS485 adaptor when connecting from a PC with Powersuite.
The pins are numbered from Left to Right when looking at the front of the drive.

CTA-ID : 2017937
Was this helpful?
What can we do to improve the information ?