Technical FAQs

Ask a Question

What are dimensions of an LH4N soft starters?

All the LH4N1 are the same size. They are 4.33 inches (110mm) tall, 4.14 inches (105mm) deep and 1.77 inches (45mm) wide.

The LH4N202** to LH4N225** are 5.75 inches (146mm) high, 4.96 inches (126mm) deep and 7.09 inches (180mm) wide.

The LH4N272** to LH4N285** are 10.03 inches (254.4mm) tall, 4.96 inches (126mm) deep and 7.90 inces (180mm) wide.

Referr to catalog 8637CT9701 for additional details.


CTA-ID : 2000742
Was this helpful?
What can we do to improve the information ?