Technical FAQs

Ask a Question

Can the NSJ600N be adjusted to provide an equivalent trip rating of 400 amps ?

Yes, setting the LO adjustment to .7 and the LR at .95 will yield (600 x .7 x .95=399) approximately 400a.


CTA-ID : 2018951
Was this helpful?
What can we do to improve the information ?