Technical FAQs

Ask a Question

Are the QOM2 load center main breakers Horsepower rated?

Squared D does not use the term ``horsepower rated``. However, the QOM2 can be used for motors when properly sized to handle the inrush current per the trip curve. See Digest 173, page 6-34 & 6-35 for other Motor protection application Data.

CTA-ID : 2018933
Was this helpful?
What can we do to improve the information ?