Technical FAQs

Ask a Question

What is the size of the transition section from 5/15kV Outdoor N3R HVL switchgear to Masterclad metal clad switchgear?

Issue:
What is the size of the transition section from 5/15kV Outdoor N3R HVL switchgear to Masterclad metal clad switchgear?

Product Line:
MasterClad.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
The transition is done in the rear of the HVL switch. The HVL enclosure is extended to be 80" deep. A 3" collar is used between the HVL section and the metal clad section. These units are front aligned. It can also be done with a 22" wide transition and a 3" collar.
Was this helpful?
What can we do to improve the information ?