Technical FAQs

Ask a Question

Are 400A main breakers hard bussed to the interior on factory assembled 400A main breaker NQOD panels?

The 400A LA main breakers are hard bussed to the interior in factory assembled NQOD panels. Also, all main breakers are hard bussed to the interior on NF panels.


Revised 6/4/04



CTA-ID : 2018344
Was this helpful?
What can we do to improve the information ?