Technical FAQs

Ask a Question

Does the ATV11 come in a 460vac range?

No, the ATV11 comes in :
100/115/120v single -phase input, three-phase output
208/230/240v single-phase input, three phase output
208/230/240v three-phase input, three-phase output


CTA-ID : 2018149
Was this helpful?
What can we do to improve the information ?