Technical FAQs

Ask a Question

Is there a 100% rated 3 pole 100 amp 480 volt breaker?<br />

Yes. LE/LX and the NJNL36150E20 can be adjusted to 100 A.



CTA-ID : 2018146
Was this helpful?
What can we do to improve the information ?