Technical FAQs

Ask a Question

How can reverse operation of the ATV58 drive be disabled?

Go to menu 4 and set Reverse Inhibit parameter rIn to Yes.
When configured for Yes, this function inhibits reverse operation even if reverse operation is requested by a summing  or PI regulator function.
This parameter is not available if a logic input is configured for reverse.  A logic input cannot be configured for reverse if this parameter is configured for Yes.
Any logic input may have already been assigned to rrS. Set the appropriate input to no (not assigned).
If operating the drive via serial communications it would still be possible to run the drive in reverse.


CTA-ID : 2018133
Was this helpful?
What can we do to improve the information ?