Technical FAQs

Ask a Question

Are QO2100BNRB, QO2125BNRB, and QO3100BNRB rated NEMA 3R? The Digest only says ``rainproof``.

Yes, these enclosures are rated for use in a NEMA 3R application.


CTA-ID : 2018925
Was this helpful?
What can we do to improve the information ?