Technical FAQs

Ask a Question

What is the ``silver`` contact rating for the 9007MS/ML.... limit switch?

120V ac: 60A make, 6A break, 10A continuous
240V ac: 30A make, 3A break, 10A continuous
28V dc: 5A resistive


CTA-ID : 2018916
Was this helpful?
What can we do to improve the information ?