Technical FAQs

Ask a Question

Is the PKGTAB Equipment Ground Bar Insulator Kit UL or CSA listed?

Issue:
Codes & Standards

Product Line:
Load Center Accessory

Cause:
Certain applications require a UL or CSA listing on the product and components.

Resolution:
This Equipment Ground Bar Insulator Kit, catalog number PKGTAB, is a UL and CSA Recognized Component Accessory. The PKGTAB does not carry a UL, UR or CSA mark. Applicable Square D load centers will list the PKGTAB on the load center labeling as an accessory.








CTA-ID : 9345
Was this helpful?
What can we do to improve the information ?