Technical FAQs

Ask a Question

Can an NQOB Column Width panel be supplied with a main breaker with a rating less than 70A, and how should it be entered in Product Selectors?

In order to supply an NQOB Column Width panel with a main breaker having a rating less than 70A, the panel would need to be entered in Product Selectors as a main lug panel with the required main being chosen as a branch breaker and specified as the main in Instructions to Engineering.


CTA-ID : 2018323
Was this helpful?
What can we do to improve the information ?