Technical FAQs

Ask a Question

What are the repair parts for the H362AWA, series F7 (may be shown as F07)?

Issue:
Current design repair parts

Product Line:
Heavy Duty Safety Switches

Environment:
Repair parts

Cause:
Maintenance

Resolution:
The repair parts for the H362AWA, series F7 (F07) are as follows. No other parts are available.
-Line Base Assembly - 4056603850 (requires one. Arc Suppressor not included)
-Load Base Assembly - 4056604050 (requires one)
-Line and Load Base Mounting Screws - 4020515101 (3 for line, 2 for load)
-Arc Suppressor Assembly - 4056635550 (requires one)
-Arc Suppressor Mounting Screw - 4020514501 (requires one)
-Lug Assembly - 4025101652 (per lug)
-Lug Mounting Screw - 4020514202 (per lug)
-Mechanism Assembly - 4056787350 (NOTE: also recommend replacing Switch Mechanism Gasket and Handle Gasket)
-Switch Mechanism Gasket - 4056786001
-Mechanism Washer - 2360200008
-Handle Assembly - 4056663550 (also recommend replacing Handle Gasket)
-Handle Gasket - 4056603101
-Lockplate - 4056672101
-Lockplate Mounting Screw - 2299940562 (2 required)
-Rod/Linkage Assembly - 4056787050
-Receptacle - WRDK6034 (mounting screws included)
-Ground Lug - 4025101652 (3 total required)
-Ground Lug Mounting Screw - 4020513503 (2 total required)
-Fuse Pullers - FPK0610 (1 required)


CTA-ID : 2018312
Was this helpful?
What can we do to improve the information ?