Technical FAQs

Ask a Question

How many analog outputs are included with an Econoflex drive with the H09 option?

There are 2 analog outputs with Econoflex drives when the H09 option is selected.
One is the AO1 located on the J3 terminal strip of the main control board. This is included on all ATV58 type drives with software versions of V5.1 and above. The other analog output is included with the H09 option.
Both outputs are 0-20 ma outputs programmable for 4-20 ma.
ATV58, Econoflex, ATV58M and FLEX58 drives with control boards with less than version 5.1 did not include the AO1 on the control board. Therefore some older Econoflex drives with the H09 option only have one analog output.


CTA-ID : 2018900
Was this helpful?
What can we do to improve the information ?