Technical FAQs

Ask a Question

What are the dimensions and weight for the ATV31HU22M2, ATV31HU30M3X, ATV31HU40M3X, ATV31HU22N4, ATV31HU30N4, ATV31HU40N4, ATV31HU22S6X, ATV31HU40S6X?

The dimensions are:
Width = 5.51 inches (140 mm)
Height = 7.24 inches (184 mm)
Depth = 5.91 inches (150 mm)
The weight is 5.19 lbs (2.35 kg)

Reviewed 6/2011


CTA-ID : 2018500
Was this helpful?
What can we do to improve the information ?