Technical FAQs

Ask a Question

What options does suffix 8099 denote in the FHL3600015M8099.

8099 in the 150a F frame Mag-Gard or automatic molded case swiches denotes the optional lug set AL100FA and the 8041 control wire connection on the lug.


CTA-ID : 2018495
Was this helpful?
What can we do to improve the information ?