Technical FAQs

Ask a Question

Can you put a shunt trip on the Powerpact Q frame Breakers?

Issue:
Can you put a shunt trip  on the Powerpact Q frame Breakers?

Product Line:
Powerpact Q Frame Breaker

Environment:
Branch breaker  in a ILINE Panel, Main or sub feed breaker in a NQ or NF panel, main breaker in a QO 3 Phase Panel, or individually mounted Q frame breaker

Cause:
Commonly use as means of emergnency disconnect for equipment like elevators

Resolution:
This feature is not available for Q frame breakers.


CTA-ID : 2018491
Was this helpful?
What can we do to improve the information ?