Technical FAQs

Ask a Question

Can the RJ-45 connector for an ATV31 or ATV28 be connected to the Ethernet connector on a computer?

No. They are not the same protocol. The RJ-45 connectors on the drives are for RS-485 communications using Modbus protocol.


CTA-ID : 2018316
Was this helpful?
What can we do to improve the information ?