Technical FAQs

Ask a Question

Does the Custom Fault for the Altivar 66 reset if Auto Restart is enabled?

Yes. If the condition that causes the fault is not present when the reset is attempted, the fault will be cleared.


CTA-ID : 2018314
Was this helpful?
What can we do to improve the information ?