Technical FAQs

Ask a Question

What is the enclosure rating for the External RFI Input Filters (VW3A58401, VW3A58402, VW3A58403, VW3A58404, VW3A58405, VW3A58406, VW3A58407 or VW3A58408) listed in the catalog for the ATV58 TRX?

IP21 and IP41.
Similar to NEMA 1.


CTA-ID : 2018301
Was this helpful?
What can we do to improve the information ?