Technical FAQs

Ask a Question

How many preset speeds can be set with the basic Altivar ATV58 drive?

4 preset speeds are used as factory default settings.
It is possible to use up to 8 presets without adding an option card.
See the keypad programming guide for additional details.


CTA-ID : 6891
Was this helpful?
What can we do to improve the information ?