Technical FAQs

Ask a Question

Does the RU3040D400CL have a main breaker factory installed?

Yes, It contains a factory installed QDL22200 feeding the 30-40 circuit intregal load center and has provisions for one more Service disconnect up to 200amp max. for field installation.


CTA-ID : 2018877
Was this helpful?
What can we do to improve the information ?