Technical FAQs

Ask a Question

What is the part number for an arm for the ZCKD17?<br /><br />

The ZCKD17 uses the ZCKY17 lever arm, which currently is available. The head without the lever attached, however, is not available as a separate part.


CTA-ID : 2018481
Was this helpful?
What can we do to improve the information ?