Technical FAQs

Ask a Question

Are the KA and KH type breakers motor rated?

Any of our breakers can be used on a motor if properly sized. In this case, motor rated is not a meaningful term.





CTA-ID : 2018479
Was this helpful?
What can we do to improve the information ?