Technical FAQs

Ask a Question

Will a CP13 and AP13 connect together?

Both the copper bars and aluminum bars are plated and the joint connectors are the same. Yes, they can be connected together.


CTA-ID : 2018472
Was this helpful?
What can we do to improve the information ?