Technical FAQs

Ask a Question

Can the 400A Class T fuses be used in the 600A EZM36600FSU or 800A EZM36800FSU fused switch?

NO. There is a physical size difference between the 400A, 600A and 800A frame size of the Class T fuses. The EZM switch will ONLY accept the fuse frame size of the respective switch (ie. 400A frame fuse in a EZM 400A switch)


CTA-ID : 2018465
Was this helpful?
What can we do to improve the information ?